Part Number: TIDA-01081
Other Parts Discussed in Thread: TPS92518, TPS92520-Q1, , TPS92515
Hi,
I wanted to discuss how inductor discharging is necessary, as I am considering both the TPS92520-Q1 and TPS92518 for generating short LED pulses, and thus was looking at this reference design.
Say we want ILED=1A, why isn't shunt dimming enough, without inductor discharging. I read that the inductor discharging was for shorter LED rise/fall times. I understand the point of precharging the inductor to 1A, but why would you discharge it? The next time you want to make a pulse, isn't it handy that the inductor current is already close to 1A? In fact, I would think the rise time of ILED when unshorting them would be much faster since the inductor already is biased near 1A just when the Qshort_led goes OFF.
Is this reference design intended to use with fast variating values for ILED? (Because I could understand a bit better why in this case)
From what I see, each time the inductor is discharged, it needs to be recharged, which somewhat limits further the LED switching frequency, doesn't it?
Thanks