Part Number: DRV2700EVM
Other Parts Discussed in Thread: DRV2700
Tool/software: WEBENCH® Design Tools
Hello,
I am looking for TINA model for the full DRV2700 part with a simple schematics. I have the TINA for the 500V fly-back, but I only need it for a 100V operation (no fly back )and I also need the amplifiers input and output pins to simulate for transient response. Can you provide the full DRV2700 model in TINA?
regards,
-ali