This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS82084: TPS82084

Part Number: TPS82084


Tool/software: WEBENCH® Design Tools

Hello

I would like to work with TPS82084 with VIN=3.3V Vout=1.8V and Iout=250mA

in datasheet its look like I can work with this DCDC to low current but on webanch I cant simulation under 0.4A.

there  is problem with low current on this DCDC?