This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP10833: Modify PMP10833 to 5Vout/1A

Part Number: PMP10833


Dear team,

Is it possible to change PMP10833 to 5Vout/1A instead of 15Vout/1A?

If this is possible, could you point out which R/L/C need to be modified?(220Vac input)

Thanks.

Regards,

Ben

  • Hi Ben,

    If you just want to change the output voltage, you can do that by just changing the output divider.

    The rest of the components can stay the same.

    Of course if you want to optimize the components, you could make some of them smaller.

    Thanks,

    Robert