Part Number: TIDA-01333
Other Parts Discussed in Thread: TVS2700
Hello TI Support,
I was reviewing TIDA-01333 front end, and got the following questions
#1 What is the maximum VIN rated for (continuous)?
#2 How is the input protected against electrical fault (Non ESD/transient related) in the event TLP3123 is ON and VIN > 10V?
if my math is correct, for VIN = 10V, R30 (0.125W) is under-rated and should be at least 0.25W assuming 20% margin.
The reason I ask is that, I am designing a similar front end.
In my case VIN_MAX = 24V, and I am thinking to add PTC to limit current in case of fault and allow for smaller sized resistor
without a PTC similar to circuit in the diagram above
- power rating for 100E / 200R are 0.75W / 1.5W respectively.
with a PTC (Itrip = 60mA)
- power rating for 100E / 200R are 0.4W / 0.75W respectively.
I came across the TVS2700 (Vclamp = 32.5V typical), but I am not sure what to make up of the DC breakdown current IBR = 12mA
#3 Does this IBR rating means that the maximum current should be limited to 12mA DC when the device is fully ON?
Thank you,
AJ