This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FREQUENCY SYNTHESIZER

Hi, 

I have a task from Analog System Lab Manual (second edition) to simulate a frequency synthesizer in TINA that will generate 1 MHz from 100 Khz output ( Experiment 7 PLL ). I made s sketch in TINA but my output readings are incorrect. Can anyvone please help. Is there problem in merging or calculation of some parameters? I try with C= 100 pF in integrator loop of VCO but it was the same. 

Thank you 

Andrea Madunic 2k.TSC