This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-010039
Wondering if this design will work down to 3-phase 208VAC L-L. If not, what would need to be changed to work down to that input voltage?
Hi Luke,
The same board can be used for 208V L-L voltage. Most of the hardware will be same (power stage) except for sensing voltage and currents where feedback and gain resistors need to be chaned, and settings on the firmware need to be adjusted to suit the new input and output levels.
Thank you
Thank you Harish.
You don't happen to know what sensor I would need. Also, I don't need an output of 800VDC. Would I need as many switches to get around 270VDC Bus?
Also, are you able to tell me where you had this built? I would like to have one built myself.
Regards
Luke