Part Number: LM3410
Other Parts Discussed in Thread: , , LM3405,
Tool/software: WEBENCH® Design Tools
Hello TI support
I looking for a LED driver for a power LED that will be used as flash to camera.
Vin to LED driver is 3.8V. (data sheet attached)
Vf of my LED is 2.85V @500mA
I would like connect 2 or 3 LED units in parallel for my application .For that, I decide that LED drive should supply up to 1A to LED and I chose - LM3410,LM3410-Q1.
1.Is LM3410 can be as good solution to my LED lighting?
2. Unfortunately i not clear understand what a different between LM3410 and LM3410-Q1.
3. Before starting of my design in purchased your EVB - LM3410XSDSEPEV because it can supply 320mA.
a. Can i play with value of R1 in order to increase LED current and get 500mA ?
4. In data sheet of LM3410 and LM3410-Q1,section 8.2.8 LM3410X WSON: Boost Flash Applicatio
You not used additional Indicator L2 that you used in LM3410XSDSEPEV (attached).
while you add that L2 to LM3410XSDSEPEV and the current is 320mA and not 1A as in data sheet? Please suggest when i need add L2 to my application?GW CSHPM1.PM_EN.pdf