This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSpice for TI installation problem

Hi, I'm trying to install PSpice for TI. I have used my email and access key as sent to me by TI when I registered. I get an error message as soon as I click sign in on the user authentication page.

The message reads "An error occurred and PSpice for TI 2020 needs to close. Refer to cdsPspiceTIlog.txt at C:...... for error details.

Here is the cdsPspiceTIlog.txt


15:11:14 21 September 2020 : Response Content length = 1527
15:11:14 21 September 2020 : C:\Users\Geoff\AppData\Roaming\Cadence\PspiceTIInstall\TI_URLs.txt bytes downloaded = 1527
15:11:14 21 September 2020 : Reading Json URL File
15:11:14 21 September 2020 : Setting TI Library URL from Json URL File
15:11:14 21 September 2020 : Reading Json URL File
15:11:14 21 September 2020 : setting media download server URL from Json File
15:11:14 21 September 2020 : Reading Json URL File
15:11:14 21 September 2020 : setting Dll path from Json File
15:11:14 21 September 2020 : Chws URL is: cdsplicwc.cadence.com/.../v1
15:11:14 21 September 2020 : DownloadServerPath is: software-dl.ti.com/.../installer
15:11:14 21 September 2020 : TILibPath is: software-dl.ti.com/.../library.zip
15:11:14 21 September 2020 : parameter count = 2
15:11:14 21 September 2020 : -wrapper
15:11:14 21 September 2020 : -CMDLINE=
15:11:15 21 September 2020 : ReleaseVersion in XML: 17.40.003 InstalledVersion on system:
15:11:34 21 September 2020 : An exception occured which is causing the program to close.
15:11:34 21 September 2020 : Details of exception are : An attempt was made to load a program with an incorrect format. (Exception from HRESULT: 0x8007000B)
15:11:34 21 September 2020 : Stack Trace for the exception is    at TIPSpice.Utilities.cdsVblRegisterInstallation(String productKey, String bundleName, String chwsUrl)
   at TIPSpice.Utilities.RegisterInstallation(String ProdKey)
   at TIPSpice.AuthWindow.AuthenticateUser()
   at TIPSpice.AuthWindow.AuthSignInBtn_Click(Object sender, RoutedEventArgs e)
   at System.Windows.RoutedEventHandlerInfo.InvokeHandler(Object target, RoutedEventArgs routedEventArgs)
   at System.Windows.EventRoute.InvokeHandlersImpl(Object source, RoutedEventArgs args, Boolean reRaised)
   at System.Windows.UIElement.RaiseEventImpl(DependencyObject sender, RoutedEventArgs args)
   at System.Windows.UIElement.RaiseEvent(RoutedEventArgs e)
   at System.Windows.Controls.Primitives.ButtonBase.OnClick()
   at System.Windows.Controls.Button.OnClick()
   at System.Windows.Controls.Primitives.ButtonBase.OnMouseLeftButtonUp(MouseButtonEventArgs e)
   at System.Windows.UIElement.OnMouseLeftButtonUpThunk(Object sender, MouseButtonEventArgs e)
   at System.Windows.Input.MouseButtonEventArgs.InvokeEventHandler(Delegate genericHandler, Object genericTarget)
   at System.Windows.RoutedEventArgs.InvokeHandler(Delegate handler, Object target)
   at System.Windows.RoutedEventHandlerInfo.InvokeHandler(Object target, RoutedEventArgs routedEventArgs)
   at System.Windows.EventRoute.InvokeHandlersImpl(Object source, RoutedEventArgs args, Boolean reRaised)
   at System.Windows.UIElement.ReRaiseEventAs(DependencyObject sender, RoutedEventArgs args, RoutedEvent newEvent)
   at System.Windows.UIElement.OnMouseUpThunk(Object sender, MouseButtonEventArgs e)
   at System.Windows.Input.MouseButtonEventArgs.InvokeEventHandler(Delegate genericHandler, Object genericTarget)
   at System.Windows.RoutedEventArgs.InvokeHandler(Delegate handler, Object target)
   at System.Windows.RoutedEventHandlerInfo.InvokeHandler(Object target, RoutedEventArgs routedEventArgs)
   at System.Windows.EventRoute.InvokeHandlersImpl(Object source, RoutedEventArgs args, Boolean reRaised)
   at System.Windows.UIElement.RaiseEventImpl(DependencyObject sender, RoutedEventArgs args)
   at System.Windows.UIElement.RaiseTrustedEvent(RoutedEventArgs args)
   at System.Windows.UIElement.RaiseEvent(RoutedEventArgs args, Boolean trusted)
   at System.Windows.Input.InputManager.ProcessStagingArea()
   at System.Windows.Input.InputManager.ProcessInput(InputEventArgs input)
   at System.Windows.Input.InputProviderSite.ReportInput(InputReport inputReport)
   at System.Windows.Interop.HwndMouseInputProvider.ReportInput(IntPtr hwnd, InputMode mode, Int32 timestamp, RawMouseActions actions, Int32 x, Int32 y, Int32 wheel)
   at System.Windows.Interop.HwndMouseInputProvider.FilterMessage(IntPtr hwnd, WindowMessage msg, IntPtr wParam, IntPtr lParam, Boolean& handled)
   at System.Windows.Interop.HwndSource.InputFilterMessage(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam, Boolean& handled)
   at MS.Win32.HwndWrapper.WndProc(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam, Boolean& handled)
   at MS.Win32.HwndSubclass.DispatcherCallbackOperation(Object o)
   at System.Windows.Threading.ExceptionWrapper.InternalRealCall(Delegate callback, Object args, Int32 numArgs)
   at System.Windows.Threading.ExceptionWrapper.TryCatchWhen(Object source, Delegate callback, Object args, Int32 numArgs, Delegate catchHandler)
   at System.Windows.Threading.Dispatcher.LegacyInvokeImpl(DispatcherPriority priority, TimeSpan timeout, Delegate method, Object args, Int32 numArgs)
   at MS.Win32.HwndSubclass.SubclassWndProc(IntPtr hwnd, Int32 msg, IntPtr wParam, IntPtr lParam)
   at MS.Win32.UnsafeNativeMethods.DispatchMessage(MSG& msg)
   at System.Windows.Threading.Dispatcher.PushFrameImpl(DispatcherFrame frame)
   at System.Windows.Threading.Dispatcher.PushFrame(DispatcherFrame frame)
   at System.Windows.Application.RunDispatcher(Object ignore)
   at System.Windows.Application.RunInternal(Window window)
   at System.Windows.Application.Run(Window window)
   at TIPSpice.App.Main()
15:11:34 21 September 2020 : Message: An error occurred and PSpice for TI 2020 needs to close.
Refer to cdsPspiceTIlog.txt at C:\Users\Geoff\AppData\Roaming\Cadence\PspiceTIInstall for error details.

Can anyone tell me what is wrong

Thanks,  Geoff