Part Number: LM5140-Q1
Hi team,
What is the maximum output current that can be achieved at both Vout1(3.3V) and Vout2(5V) when the input is 12V,
Thanks
Mahendra
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5140-Q1
Hi team,
What is the maximum output current that can be achieved at both Vout1(3.3V) and Vout2(5V) when the input is 12V,
Thanks
Mahendra
Hello
The governing factor regarding the max Iout for a controller is
how large a FET it can drive. Larger Iout means larger FETs with larger gate drive power required.
That means more power dissipation in the controller and a slower gate drive for the FETs. The gives less
efficiency and higher temperature rise in the application.
Your best way to design your application is to use the calculator tool on the TI product page for this device and/or Webench
to experiment with FET sizes vs power dissipation and efficiency.
Thanks
Hello
I will close this post due to inactivity.
You can re-open if you have more questions.
Thanks