Part Number: TPS55340
Other Parts Discussed in Thread: LM5157
Hi Team,
I would like to get assistance why the values below of our customer is cannot generate a design in Webench for TPS55340:
Vin, min. = 6V
Vin, max. = 24V
Vout = 16V
Iout = 1.2A
I also tried the values on page 22 in the datasheet since the customer will implement a SEPIC application and also cannot generate a design.
Can you confirm if TPS55340 still a good choice for the customer requirement above as this is within the range of TPS55340 but cannot work in Webench tool?
Thanks,
Jonathan