This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Short Circuit Current Detection



Hi

I am working on the Battery Application ( 0 to 100VDC) and measuring the charge / discharge 100A current with shunt method. Now I want to introduce the short circuit detection and protection of power switches. The permissible short circuit current is ~400A for few micro seconds. Please suggest how to detect this current  <10uS.

Thanks

Sandeep