Part Number: TIDA-01634
Hello,
However, the board is "not availabale for sale" - how can I still get it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01634
Hello,
Hello Karl,
Please refer to the attached thread.

Regards,
-Mamadou
Hello Mamamdou,
thanks for the reply.
Yes, the suggested alternative is nearly the same. The difference is the EPC2001C with limitation to "only" max. 10MHz. I will check this in detail.
What do you think: Would it be possible with the suggested board to switch 40..50MHz for 500ns within a repeted cycle of 25µs?
Do you know, if a pure TIDA-1634 board (without assembled parts) would be available?
Regards
Karl
Hello Karl,
A modified version of the suggested board may handle higher switching frequencies with the appropriate FETs (typically smaller FETs) and the appropriate thermal management considerations including heat sink, forced air, grounding, etc...
I have not physically come across the TIDA board and these are generally intended to show the IC's functionality in a system level configuration.
I suggest using the EVM design files and updating them according to your desired application.
Regards,
-Mamadou