Tool/software: Code Composer Studio
I made a design of an inverter with a processor: TMS320F280049CPMS.
1-
What is the maximum rotation frequency on this processor ...?
2-
Do you need to modify three RC filters of three phases that the processor measures ...?
Now I have a resistor with phase = 100k and a 100nF capacitor and a 6k resistor to ground. Is it possible to reduce the capacitor 100nF and to what the lowest value to correctly measure the phase voltage ...?
3-
I used PWM = 20kHz
I need a motor rotation frequency of 1200Hz.
Is this frequency possible and do I have to modify the phase voltage filters ...?