This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01168: optimized layout

Part Number: TIDA-01168

Greetings -

Please let me know if information is available regarding the optimized layout mentioned in "TIDA-10068: Board Size Information", January 22, 2019.

"I have an experimental design with LM5170-Q1 in works which has 31 x 51mm state-of-the-art powerstage rated for cca. 600W. Additionally, an analog control with the LM5170-Q1 is on the four-layer PCB with single-side component placement which is 62 x 51mm. I shall be ready to publish data 2Q/2018."

- Bruce

  • Hello Bruce, 
    I never managed to publish the design on TI.com. My assignment & team priorities had changed right about the time of finalizing the design. I will reach out to you using a personal message. Please accept the requested connection on the E2E forum.

    Best regards, Jiri