Tool/software: WEBENCH® Design Tools
Dear Sir ,
Kindly send me the simulation model for the XTR105 PT100 to 4 to 20 mA transmitter
so that I can use the file in the TINA software
with best regards
K. Ganapathy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Dear Sir ,
Kindly send me the simulation model for the XTR105 PT100 to 4 to 20 mA transmitter
so that I can use the file in the TINA software
with best regards
K. Ganapathy
Hello,
Unfortunately there is not an official SPICE model for the XTR105. There is an unofficial model that's been created to help understand the transfer function and connections to the XTR105, however they do not model the performance metrics of the XTR105. The ideal op amps used in the design can create unrealistically large voltages and currents so if you notice something strange there's probably a connection issue. I'm attaching the model here, but you can also refer to this original post where the model was shared for more details.
Hi Many thanks
I will get back if any further questions
best regards
K, Ganapathy