This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSPICE-FOR-TI: How to add spice model

Part Number: PSPICE-FOR-TI

Dear representative

Hello I want to add BZT52C12T.spice.txt to pspice for TI but could I ask you how I can do it?
(ZT52C12T.spice.txt is in below link)

https://www.diodes.com/search/?q=BZT52C12T.&t=keyword&action_results=Go

*SRC=BZT52C12T;DI_BZT52C12T;Diodes;Zener 10V-50V; 12.0V  0.500W   Diodes Inc.
-
*SYM=HZEN
.SUBCKT DI_BZT52C12  1 2
*        Terminals    A   K
D1 1 2 DF
DZ 3 1 DR
VZ 2 3 9.78
.MODEL DF D ( IS=17.2p RS=32.5 N=1.10
+ CJO=42.7p VJ=1.00 M=0.330 TT=50.1n )
.MODEL DR D ( IS=3.43f RS=9.46 N=3.00).ENDS