Other Parts Discussed in Thread: TIDA-01494, , UCC28740, UCC28951
Hello Ti,
I want develop custom smps board with TIDA-010015, or TIDA-01494 + TIDA-0153.
I have some questions about output voltage.
I need 48v output (450w will be enought) to chargue bateries and I have read in the specifications for this Tida: "The output voltages from these supplies
range from 5 to 56 V with power ratings from 7.5 to 480 W", so I think that is it possible doing several changes in Transformer, diodes, capacitors and
feedback loop circuit to get it.
If the project work well, we could insert this board in all our equipment.
Please could you support with these circuit modifications?
Maybe there is another Tida circuits more appropriate for 48 volts output. ¿?
Thanks a lot!
Regards