This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS61372: Inrush current estimation

Part Number: TPS61372
Other Parts Discussed in Thread: LM2735

Tool/software: WEBENCH® Design Tools

Can you tell me what would be the inrush current based on the Webench report attached below

6864.24V 120mA 85C LM2375YQ1.pdf

Some parameters for the above report are as follows:

Vout: 24V

Input voltage range: 3.3V to 3.7V

Iout max: 30mA