Several of the TI parts that I want to use in a simulation are not in the PSpice for TI libraries. How can I import the missing models into PSpice? I have looked at the importing models video, but the TI parts already have .lib, .opj and .dsn files and also a separate library directory with a single .olb file. An example is the TPS7A4501-SP part.
I have three questions:
1. How should I copy/import these files into PSpice for TI?
2. Since they are being copied/imported in to PSpice for TI will they count to the limit of three imported models which limit the functionality of PSpice for TI?
3. When will the missing models be included and how can I request for a TI model to be included in the PSpice libraries?
Thanks
Steve