This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using a model created for PSpice. Yet during simulation, an error message showed up saying only three probes are allowed. I see one of the following errors:
ERROR(ORPSIM-16583): Detected an imported model containing transistors or diodes. For such models, PSpice for TI supports a minimum of one and maximum of three traces. Reduce the number of traces and simulate again.
ERROR(ORPSIM-16583): Detected an imported model containing transistors or diodes
INFO(ORCAP-15098): Detected an imported model containing transistors or diodes. For such models, PSpice for TI supports a minimum of one and maximum of three markers.
What does that mean?
If you are using an imported model, PSpice for TI is subject to probing limitations during simulation. Using a third-party model will limit the tool to a maximum of three probes. If you need more than three probes, there are multiple solutions:
Please do not manually import TI models. To ensure that all built-in libraries are up-to-date with the latest models, PSpice for TI will automatically check for updates or new models. A "Library Update" popup will notify you of any updates.
Please select "Yes" to update. Selecting "Always apply library updates" is also recommended so you don't need to click "Yes" manually. If you select "Not at this time," you will not have the most up-to-date models. If you are still experiencing probe limitations with TI models, or cannot find the TI models within the tool, please make a post in the TI E2E. This may be an indication that we need to update or modify our model.
If you are still experiencing trouble, please click here to open a new thread on the PSpice for TI E2E forum.