Other Parts Discussed in Thread: UCC28730
My design input voltage is range from 70V~120V, and the output expected to be 5V, load is about 50mA, applied for automotive
1. Is it ok to bear from 70~120V input for PMP22557
2. Is it ok to change the PMP22557 to 5V output ? how to change
3. I see UCC28730 is for a flyback controller , but it looks like the PMP22557 is not designed as a flyback, is that ok?