Part Number: TIDA-01623
Other Parts Discussed in Thread: UCC28780
TIDA-01623 connot start,
PFC is OK,
ACF: Vo=0V,
I don't know what kind of protection is trigged.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01623
Other Parts Discussed in Thread: UCC28780
TIDA-01623 connot start,
PFC is OK,
ACF: Vo=0V,
I don't know what kind of protection is trigged.
Hi Sanhe
since there is no PCB/Schmatic available, i could not identify the root cause, basically, you should check the polarity of the transformer Aux winding is correct or not, for IC related debug issue, you can also reach out to UCC28780 product line for more comment.
BR
Max
Hi BR
This place doesn't seem to be able to insert files.I'll upload it first,I wonder if you con see it.
A good day!
Youyi Yan SanHe Laserconn100W12V.PCB100W12V.pdf
Hi,
as i know it is not a good place to show customer schematic and PCB, can you send the file to my TI working mail, m-wang1@ti.com
thanks
BR
Max