Part Number: PMP10531
Other Parts Discussed in Thread: TIDA-00199, LM5160
Hi,
I am working on a TIDA-00199 IGBT supply. And in that circuit I made a few modifications such are:
- Vin = 15 V
- Transformer Secondary rated at 25volt/300ma
- R2 is 110K and R6 is 13 K for UVLO Level.
- All the output capacitor (10uF) I used is electrolyte instead of ceramic.
It works fine under no-load condition but when I am connecting a load it shut of and output voltage has gradually down to 8 volt and -5 volt
I connected a 300ohm resistor across all 8 output (+15v to GND and -10Volt to GND)
My question is:
- Can this design work on 15volt input voltage with this transformer too?
- Is there any modification required in the attached Schematic?
- why load regulation is poor? am I missing something important?
For your reference, I am attaching the Schematic, Transformer detail as well. Please review this and share your valuable feedback.
SANHE-20-xxxchenrenshu20.11.26.pdf