This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01580: What components are needed to build an ecg circuit?

Part Number: TIDA-01580
Other Parts Discussed in Thread: TIDA-00096, TIDA-010029

Hi! I am trying to determine which circuit is best for a senior design project and am confused as to what parts are needed to build a circuit for an ecg application. We are deciding between the TIDA-01580, TIDA-00096, TIDA-010029, and the circuits that use the MSP430G2 launchpad (https://www.ti.com/lit/an/slaa280b/slaa280b.pdf?ts=1612299021019) Looking through the documentation it looks like an AFE, MCU, and Boost converter are needed for all of these circuits and need evaluation modules to get them operating? If there is anyone I can talk to/connect with to figure this all out that would be greatly appreciated.