Part Number: PMP4311
Other Parts Discussed in Thread: UCC28070, UCC28180
Hi,
for a current PFC project, I am considering switching to UCC28070 controller.
In the test results for PMP4311 design THD is only mentioned for 220V @100% load (<8,7%) and 180V @100% (<6,9%).
Do you have some furhter information on THD at high line (264V) and also low load condition (e.g. 25%, 50%, 75%).
Thank you very much
Julia