Part Number: TIDA-01455
Hi Team,
Greetings, We need your help to check customer's concern below.
----
There are two things that catch my eye in the TIDA-01455-E1 (001) _TI-BOM.pdf list.
A. Listed as Q1;
1200 V
IGW03N120H2
Infineon Technologies
Transistor, IGBT, 1200 V, 9.9 A, TO-247
TO-247
why was the product above used?
B. In the same list of materials; C50, C51
listed as;
3uF
MKP1848C53012JK2
Vishay-Bccomponents
CAP, Film, 3 μF, 1200 V, +/- 5%, 0.015 ohm, TH
32x18mm
there is a capacitor. this is like the q1 transistor, 1200V.
Does it have any special meaning to be 1200V? Because other system components max 600V.
But these 3 materials; (q1, c50 and c51) 1200V is selected.
What will happen if a value such as 450V is selected as a capacitor? because of the high pwm frequency anyway, the back emf will be very low.
---
Thank you in advance for the support.
Best regards,
Jonathan