Other Parts Discussed in Thread: CD4016B
I'm trying to use an IC bus chip, to provide a switching solution. We had "Black Box" make us a selector switch, that isolated incoming Cat 6 connections to microphones. The Black Box switches mechanically fail very quickly. We use a set of (4) microphones, at 4 different distances, to provide our targeting or dispersion of ammunition. The microphones find the location of apparent bullet coordinates, much the same as a computer mouse coordinates are arrived at. The signals from the microphones are amplified to +15VDC. The different target locations need to be isolated for different range tests. I was hoping I could use the SN74CBT16245DL to be the "Switches" in a circuit, that might do the same thing as the mechanical "Black Box" switch set up. We would use a logic 1 or other signal to operate the transfer of the incoming +15VDC signals to connect to the chips output for the different incoming target signals. I'm having trouble finding a prototype board to solder the IC to. It appears to have a pitch of .035" (.889mm). I would need a breadboard that could service at least (3) of these IC's, and possibly other logic and passive components. Any idea's?