This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01426: Analog DCAC solution using TL494

Part Number: TIDA-01426


Hi team,

Customer wants to use this reference design in their DCAC project. They want to use total analog device to achieve DCAC.

The requirements are shown as below:

  • Input: 3s Li battery;
  • Output: 220VAC
  • Output power: About 100W.

Can this reference design be used in the project if using suitable MOSFET and transformer? Or is there any better solution? Thanks.