This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01385: CT recommendations, primary current

Expert 6470 points
Part Number: TIDA-01385


Team,

in this design we are getting from 3mA to 2A:

  1. Do we have some references what kind of CT was used in that setup?
  2. What was the primary current? 

We are getting much lower values than that, if you can direct us in the right direction it would be very helpful.

Thanks.