Part Number: TIDA-00548
Other Parts Discussed in Thread: ADS1263
Hi,
Iam plan to use TIDA0058 evaluation board based components and schematics for my design. Please clarify below queries
1. The board having SIL3 certification due to the hercules series MCU only? Analog circuit section including ADS1263 have any SIL certification(As because in our design MCU not using, but we need SIL certification)?
2. a. The evaluation board uses ADS1263 IC for analog input function. The IC datasheet showing the analog input pins are tolerant up to 7V. Then why in evaluation board it is saying 33V tolerant?
b. By feeding 24V to one end of Rsense pin another end will connect to load. Will this work?
3. whether using ADS1263 can we able to sense current from 0 to 120mA?
Kindly consider this as urgent and reply
Warm regards,
Monisha OM