Part Number: TIDA-010056
Hello Team,
We are getting voltages on output side. We have connected lamp load as 3 phase. But when we are are varrying potentiometer we can't see change of pwm duty cycle. We have connected lamp load as 3 phase. Ideally when we are varrying potentiometer brightness of the lamp should be decrease. But it isn't. Hall sensor signals we are generating using Arduino Due (50% Duty cycle and 120 phase difference 3 phase ) .Driver IC is used DRV8353RH. Code we are using provided by TI for TIDA-010056. While debugging of program code we find that SPEED_REF variable used in code is not changing when we are varying potentiometer. To check SPEED_REF adc pin working or not , We had written single code to read SPEED_REF as ADC and it was working properly. But in our main code it is not changing.
Please help us to solve this problem.
Thank you in advance.