Part Number: TIDA-01622
Hi Team,
Good day.
I have a question about the BOM on the TIDA-01622.L3 in the BOM does not fit to the actual foot print on the board.
Part number: 744822120
Designator:L3
Package Reference: 17 x 12 x 20.5mm
Kindly check if this p/n would fit as it should be or it might need a replacement? Thank you.
regards,
Jonathan