Hi,
There is a new parameter GAPBOND_ALLOW_DEBUG_KEYS in the latest SDK v5.10, and I want to verify this configuration.
I download the simple_peripheral demo from SDK v5.10, and make sure the GAPBOND_ALLOW_DEBUG_KEYS is true (default value is true), to a TI LaunchPad(A).
and I download the simple_central demo from SDK v4.40 and set the GAPBOND_SC_HOST_DEBUG true (default value is false), to another TI LaunchPad (B).
Then I can connect A and B, read RSSI value and run GATT write.
That's correct. But after I set the GAPBOND_ALLOW_DEBUG_KEYS value to false in Pad A, B can connect and communicate with A as well. Nothing difference after I change the value of GAPBOND_ALLOW_DEBUG_KEYS.
I am not sure whether this parameter (GAPBOND_ALLOW_DEBUG_KEYS ) will be checked during the connection establishment or pairing/bonding time. How Can I verify the change of this parameter?
Cheers,
Ming Sun