Questions are as follows:
1. The chip cannot be automatically reset for the reset command sent by the Android APP, while the IOS can.
2. In the process of upgrading through OAD, if the chip is powered off and re-powered on again, the chip cannot operate normally, it can only be done after re-downloading the program through the burner.
3. After the chip is upgraded through OAD, the content previously written in the flash is gone.