I need to use an internal RC oscillator, but the accuracy is not enough.
Refer to the method in the link below and use the function HCI_ EXT_ SetSCACmd(); When SCA is set to 0,40500 and tested for 60 seconds, the deviation is about 0.04s, which is equivalent to 666ppm.
software-dl.ti.com/.../custom-hardware.html -32-khz-crystal-less-mode
666ppm is obviously unacceptable.
Is SCA not set successfully?
How to determine whether the setting is successful?
Is there any other way to improve the accuracy of the internal RC oscillator?
test with simple_ peripheral_ oad_ offchip.
This problem involves a large number of orders that we have shipped, hope to help me solve it as soon as possible, thank you!