Dear TI expert:
==== My code enviroment showed as following ====
My SDK version is : 3_40
IDE Tool: CCS 9.1.0
Using Example: examples\rtos\CC2640R2_LAUNCHXL\ble5apps\simple_serial_socket_server
==============================================
Description:
I use the mobile phone App named "Bluefruit Connect" to scan the TI CC2640R2F.
But the address field always different after I restart CC2640R2F.
Is this a normal situation? The address is the BT MAC Address? It seems different with the MAC address which I read from the "Flash Programmer 2 Tool"
Or it is a special function?
Thanks!