Part Number: CC2564C
Other Parts Discussed in Thread: CC2564,
Hi,
I'm wanting to have low latency audio through the CC2564 using A2DP profile. I'm using an MSP432 running the Bluetopia stack to interface with the CC2564. The CC2564 is configured to put the audio out its I2S audio interface. At the moment, using my Bluetooth analyzer, I'm measuring about 100ms of latency between the audio packet in the air to when it appears at the speaker. Using a MAX9880A as my codec.
I'm hoping this latency can be reduced significantly, but it's not clear what parameters of SBC or A2DP I need to tweak to help reduce this delay.
Thanks for any help.
Jason