Other Parts Discussed in Thread: CC2640
Tool/software: Code Composer Studio
SDK --> simplelink_cc2640r2_sdk_4_10_00_10
I am working on "Simple peripheral" project.
BLEstack -> Simple peripheral
-----------------------------------------------------------------------
Hi,
Description of my application:
Normal Simple peripheral example code is used on top of that ANCS example code from GitHub is integrated.
1. The Data transfer via ANCS is happening correctly and Call missed call, SMS, etc notification is received on the BLE side also.
2. I am also trying to send data from the iOS phone side via GATT characteristics also, the data transfer here also is happening seamlessly.
ISSUE:
Now, when I am trying to disconnect from the ios app & BLE then the disconnect is shown just in-app, not proper disconnect is happening.
The connection is still established b/w phone and BLE from behind (checked in phone's Bluetooth section).
Observation:
When I am taking back the ANCS changes and connecting the iOS app & BLE the disconnect from the app is happening as expected.
What can be the issue here?
Need to get it fixed ASAP.
ANCS code imported from the below example in GitHub:
Regards,
Saurav