Part Number: LP-CC2652RB
I would like to utilize the LP MCU in a project off a battery but the LP draws about 130mA itself (powered from USB). That's obviously the easiest power input from a power pack... I don't see any good hack to disable the XDS circuit but want to make sure there's not something I'm missing—is there any way to power the MCU from the USB input without that current draw?
I'll need to regulate power myself if I move off-board which starts to become a new project (pain). Thanks,