Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2650
Tool/software: RF Studio
SDK --> simplelink_cc2640r2_sdk_4_10_00_10
Our test lab agency will be using Interlab Bluetooth radio tester for RF PHY testing. we want to figure out HCI communication options.
Is below required command can be set with Interlab Tester with the help of XDS110 debugger?
a) LE reset
b)payload length
c)TX/RX frequency
If Interlab Bluetooth radio tester is not supported by XDS110 debugger, then other option by RF studio application with debugger usage. Is this the correct option for HCI communication? What are the option/command available to set LE reset, payload length, TX/RX frequency?
Also attaching mail communication with more backup.
[EDIT] E2E is a public forum. Please do not attach internal email communication. Thanks. Clement