Part Number: CC2640R2F
Hello,
my question can be broken down into two parts.
Firstly, I want to measure the power (current) consumption of a simple application I am developing using a Launchpad board. For this, I have taken the pinStandby application provided by TI and it works fine. I have removed the jumper over the GND pins and have routed the signal through a multimeter. I can measure a standby current of around 2mA which goes up slightly if the LEDs are ON. I am using the RTOS variant of the example. Is this value correct?
Second. I see that the RTOS supports a Standby mode for the chip. I could not find a simple example to test this. Ideally, I would like to see the chip draw a fraction of a mA to verigfy that it has indeed entered the Standby mode. I have read about modifying the examples to enter the Standby mode but could not get it to work. Could someone provide a simple step by step guide to verify the Standby mode or point me towards an existing solution? The tools I am using are standard, a Launchpad and a multimeter and no custom boarsd or similar.
Regards,