This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Adding Scanning to SimplePeripheral

Part Number: CC2640R2F


Hello,

Chip: CC2640r2f

SDK: simplelink_cc2640r2f_sdk_4_20_00_04

I would like to alternate between scanning and advertising on a fixed time interval.

I have adverting on a fixed interval working using the SimplePeripheral Project.

I have scanning on fixed intervals working using the SimpleCentral Project

I've spent sometime trying to add the "other" feature to each project and haven't had much success. Adding scanning to SimplePeripheral, I have a project that will load ontop the chip but GapScan_enable return 0x12 which I believe means there's something wrong with my configuration. I plan on digging into this more today but wanted to throw the question out there while I triple check my setup.

Is there a better starting point that would get me scanning and advertising in the same project?

This should be possible to scan and advertise within the same project correct?

Any info or insight is appreciated.