This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: SCS Run-Time Logging "Data structure signatures not received from target"

Part Number: CC2650MODA
Other Parts Discussed in Thread: BOOSTXL-CC2650MA

Hi all,

I am working with the BOOSTXL-CC2650MA connected to the debugger through the JTAG connector. I am trying to work with Sensor Controller Studio to work with the ADC. However, I am having issues with testing my code with the Run-Time Logger. When I hit the Connect button I receive a "Data structure signatures not received from target" error. 

I cannot seem to figure out what the issue is. 

Initialization Code:

// Select ADC input

adcSelectGpioInput(AUXIO_A_INPUT_PIN);

// Set up the first timer trigger ~100 ms from now

evhSetupTimer1Trigger(0, 100, 2);

Event Handler A Code:

// Enable the ADC (fixed reference, 2.7 us sample time, manual trigger)

adcEnableSync(ADC_REF_VDDS_REL, ADC_SAMPLE_TIME_2P7_US, ADC_TRIGGER_MANUAL);

// Sample the sensor and store the ADC value

for(U16 n = 0; n < BUFFER_SIZE; n++) {

adcGenManualTrigger();

adcReadFifo(output.samplingBuffer[n]);

}

// Disable the ADC

adcDisable();

// Log the output samplingBuffer

rtlLogStructs(BV_RTL_LOG_OUTPUT);

// Next event triggers in 5000ms

evhSetupTimer1Trigger(0, 5000, 2);