Other Parts Discussed in Thread: CC2640
CC2640 problem description:
1. Chip model: CC2640R2FRGZ
2. Phenomenon:
Product 1: Bluetooth Beacon device, broadcast data at 220ms, directly powered by disposable lithium battery, full battery voltage 3.66V.
Problems: (1) When the equipment is power-on, the power cord needs to be welded. The back and forth contact between the welding pad and the power cord is bad, resulting in the chip not running. There is no output of 32.768K crystal oscillator in the test.(2) The Bluetooth beacon device has data detected before delivery, but a small part of it will crash after on-site installation. Some will crash after a few days, some after a few months, and there is still no output of 32.768K crystal oscillator back to the factory for testing.
Product 2: scanning beacon data equipment, rechargeable lithium battery through LP5912-3.3DRVT voltage stabilization to power the chip, lithium battery charging chip is BQ24040DSQR.2S turn on 260ms scan beacon to broadcast data.
Problem phenomenon: When 2 80 products were put into the temperature cycle chamber to do the temperature cycle experiment at -10~+55℃, 20 CC2640R2FRGZ were found to crash 48 hours later, and there was no output of 32.768K crystal oscillator in the test.
3. When the above two products crash, both can cut off the power supply, discharge the capacitor on the PCB and then restart the power supply.If the power supply is cut off without discharge operation, the restart is invalid.Doubts whether the chip dies under the low power consumption, hopes to assist the analysis, thanks!