Part Number: CC2652R
Other Parts Discussed in Thread: UNIFLASH
Hi All,
I am using CC26x2 launchpad, on that i am using multirole example from SDk 5.10.
I have followed the steps mentioned in Enhanced OAD from this link:
https://dev.ti.com/tirex/explore/node?node=AIixxGE2y6tnPJ7cm65SFQ__pTTHBmu__LATEST
All steps completed ,output oad.bin also generating.
I am trying oad unsecured and relese configuration.
But when i try to load that file using uniflash after loading bin file selecting load Addr:0x00000000
loading finishes but device does not boot.
but the when i debug same project and run the application device boots and starts advertising.
So two inputs which might be helpful for my issue.
1.Instead of uniflash if i want to load firmware using Flash Programmer-2 what is the procedure.
2.what might cause device not to boot when flashed but working with same code in debug?
Regards,
Atul