This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: Error while entering debug mode in CCS 10.4

Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: UNIFLASH

Hello,

I'm facing the following when i tried to enter debug mode in CCS IDE

Error initializing emulator:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.
(Emulation package 9.4.0.00129)

i have tried with different USB ports as well as cables, does CCS automatically update the serial number or do i have to update it manually using xdsdfu?