Part Number: CC2564C
Hi Team,
Need your expertise for our customer's query. We're aware that CC2564C can connect to 7 devices over BT. My question is do I have to setup an intercom kind of set up? Thinking of it as a local phone system over Bluetooth in a 10m room. I need to connect to different devices to speak one to one.
One possibility we are thinking about is keep connected to all the devices over BT (with HFP profile), and make the eSCO channel (Audio) only to the device we want (like dialling a call) Would this be possible?
If that is not possible. Can you help us on possible solutions to achieve the above case?
Just for background info, we are using CC2564C in Dual mode with BT-BLE support with Bluetopia stack for STM32 uC. For audio we are using unassisted-HFP and A2DP modes, and we already have HFP examples working.
Thanks in advance!
Kind Regards,
Jejomar