This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652RSIP: Bluetooth stack

Part Number: CC2652RSIP

Hello,

I work for Viveris Technologies and we are interested in using your reference CC2652RSIP for one design.

Project context :
- Application : confidential, audio data transfer (full-duplex)
- Constraints : Operating temperature = -40°C/+85°C, low energy consumption (portable device)
- Development phase : Q4/2021 to Q4/2022
- Start of production : 2023 = 1K pcs
- Production : ramp-up to 10K pcs/year for at least 7 years

We have some questions about the Bluetooth stack:

1. How is it delivered, source code or compiled binary file ? Is it free of charge or is there any fees to pay for the BT stack ?

2. Can the Bluetooth stack be freely modified in order to :
- Remove the pairing over the air, add pairing through local MCU for security purposes
- Guarantee full duplex communication (talker/listener at the same time)
- Guarantee multi-profiles (HSP/HFP/A2DP emission, ADFP reception, SPP/AVRCP...) support with fast changes from a profile to another

3. What would be the impact of such modifications on the Bluetooth certification ?


Do not hesitate to come back to us if your need more informations about these specific needs.

Best regards,

Ambroise CHAIGNE, Viveris Technologies