This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 - information required

Other Parts Discussed in Thread: CC2540, CC-DEBUGGER

I have recently purchased the IC-CC2540. Also I am very beginner to use this ic. It will be very helpful If u can help me regarding the following topic.

I want to develop bluetooth connectivity with with Cell Phone for sensing application. I will connect a sensor to CC2540 in its analog input pin, & it will transmit sensor reading to a cell phone.

queries 

1. Which pin are the Analog input pin that goes to ADC for A-D conversion.

2. What are the hardware required to program the CC2540.

3.  How to make the program. i.e. is there any code composer studio for programing the cc2540.

4. In the datasheet I did not found  any application note which includes a typical application like sensor interfacing (as an example, typical application note for a TI instrumentation amplifier includes different sensor interfacing ). 

I request you to help me , providing the above required information.

  • Biprangshu Saha said:
    1. Which pin are the Analog input pin that goes to ADC for A-D conversion.

    Please see section 7.6 of the CC2540 User Guide (http://www.ti.com/litv/pdf/swru191b)

    Biprangshu Saha said:
    2. What are the hardware required to program the CC2540.

    The CC Debugger (http://focus.ti.com/docs/toolsw/folders/print/cc-debugger.html) allows you to program a CC2540 device. An easy way to get up and running is to purchase the CC2540DK-MINI (http://focus.ti.com/docs/toolsw/folders/print/cc2540dk-mini.html), which includes a C2540 USB Dongle, keyfob board, and a CC Debugger.

    Biprangshu Saha said:
    3.  How to make the program. i.e. is there any code composer studio for programing the cc2540.

    You will need IAR Embedded Workbench for 8051. For more information on the software requirements, please take a look at the CC2540 SW Developer's Guide (http://www.ti.com/litv/pdf/swru271)

    Biprangshu Saha said:
    4. In the datasheet I did not found  any application note which includes a typical application like sensor interfacing (as an example, typical application note for a TI instrumentation amplifier includes different sensor interfacing ). 

    The sample applications in the software development kit should help you with this.

  • I have downloaded IAR Embedded Workbench for 8051, v. 7.51A, Evaluation edition, as mentioned in  (http://www.ti.com/litv/pdf/swru271) document. But while installing the EW8051-EV-751A.exe, it is showing some error  

     

    Component IAR Embedded Workbench MCS-51

     

    File Group File Group 2

     

    File C:\ Program Files (x86)\IAR System\ Embedded Workbench 5.3 Evaluation version\8051\src\lib\wcs5713.tmp

     

    Error Access is Denied  

     

    I am using windows7.Does it have any compatibility issues with windows7 if so what should i do.